You are here: Using KAS Simulator > Start KAS Simulator

Start KAS Simulator

To start the KAS Simulator perform the following actions.

  1. Click on the Start menu
  2. Select All Programs
  3. Click Kollmorgen > Kollmorgen Automation Suite > Kollmorgen Simulator.

The first time Simulator is run it will attempt to open some TCP/IP ports to allow communication. Your system's firewall will detect this and prompt for an action. Allow the Simulator to open the ports by selecting Unblock (Windows XP) or Allow Access (Windows 7).

Figure 6-1: Firewall alert dialog.

 

Log Window


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™